AXIS#.MOTOR.SERIALNUM

This parameter is the motor serial number.

 

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

 

General Information

Type

Read

Units

N/A

Range

14chars

Default Value

empty

Data Type

String

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.SERIALNUM

6242

1862

String

Read Only

-

AXIS2.MOTOR.SERIALNUM

71778

1186

String

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.SERIALNUM

6242

String

Read Only

-